Edit a zone

Edit the properties of a zone to specify a name, description, and enable security settings.
  1. From the navigation bar, select either:
    • Canvas
      and then select a zone.
    • Zones
      and then, next to the zone, select
      Properties
      .
      TIP: You can also select
      Overview
      and then select a zone from the list.
  2. Make edits to
    ZONE PROPERTIES
    .
    For more information, see Zone properties.
Add devices to the zone. See Devices.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal