Add a zone

Add zones to establish areas of security policy. Devices assigned to a zone trust each other.
  1. From the navigation bar, select either:
    • Canvas
      and then select
      Create New
      Zone
      .
    • Zones
      and then select
      Add
      next to
      ZONES
      .
      TIP: You can also select
      Overview
      and then select
      Add
      from the toolbar.
  2. Make edits to
    ZONE PROPERTIES
    .
    For more information, see Zone properties.
Add devices to the zone. See Devices.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal