Edit a range

Edit the properties of a trusted IP addresses range.
  1. From the navigation bar, either:
    • Select
      Canvas
      .
    • Select
      Zones
      and then select a zone that contains the range.
    • Select
      Devices
      .
  2. Select the range to edit.
  3. Make changes in
    RANGE PROPERTIES
    .
    For more information, see Range properties.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal