Range properties

Use range properties to define pools of IP addresses that can be used to permit unsecure communication within the policy model.
IMPORTANT: Add IP addresses only for devices that are intended to originate connections. Limit the usage of this method as it deteriorates the level of security of the system.
Properties
Property
Description
Name
The name of the range. The name is required and must be unique.
Description
An optional description for the range.
Start IP Address
The first IP address of the range.
End IP Address
The last IP address of the range
Zone
The security zone to which the range is assigned.
TIP: If you add a range from within the
Zone
list, the range is automatically assigned to the currently selected zone.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal