Add a range

Configure a trusted range of IP addresses that are known to contain good devices.
  1. From the navigation bar, select either:
    • Canvas
      and then select
      Unassigned
      or a zone to contain the range.
    • Zones
      and then select a zone to contain the range.
    • Devices
      to add a range unassigned to any zone.
  2. Select either:
    • In
      Canvas
      , from the toolbar, select
      Create New
      Range
      .
    • In
      Zones
      or
      Devices
      , from the toolbar, select
      Add Range
      .
  3. Make changes in
    RANGE PROPERTIES
    .
    For more information, see Range properties.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal