Add a conduit

Add a conduit to connect two endpoints. An endpoint can be either a device or a zone.
  1. From the navigation bar, either:
    • Select
      Canvas
      and then select
      Create New
      Conduit
      from the toolbar.
      TIP: You can also right-click a zone, device, or range and then select
      Add Conduit
      .
    • Select
      Conduits
      and then select
      Add
      from the toolbar.
  2. In
    CONDUIT PROPERTIES
    , under
    Endpoint 1
    , select
    Browse
    .
  3. Select a zone or device to assign as the first endpoint of the conduit and select
    OK
    .
    TIP: Use
    Filter
    to find endpoints.
  4. Under
    Endpoint 2
    , select
    Browse
    .
  5. Select a zone or device to assign as the second endpoint of the conduit and select
    OK
    .
  6. Select
    Next
    .
  7. Make changes in
    CONDUIT PROPERTIES
    .
    For more information, see Conduit properties.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal