Syslog routing

Use Syslog routing to configure the logging of messages that are sent between devices.
The Syslog routing service requires a Syslog server to operate. The Syslog routing policy is applied to every device in the policy model that supports Syslog routing.
To enable, disable, or configure Syslog routing, see Edit Settings.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal