Unexpected changes in a safety project

When the safety content of a project is not the same as when the project was last closed, FactoryTalk Design Studio detects the unexpected changes. The integrity of the safety application may have been compromised, and you should verify the safety content. Use the
Uncommitted changes
dialog to view or discard the unexpected, uncommitted changes.
To view unexpected and uncommitted changes
  1. Select
    File > Source control > Uncommitted changes
    , or on
    Change history
    , double-click an uncommitted change.
    TIP: The
    Uncommitted changes
    menu option appears only if there are saved but uncommitted changes in the project.
  2. In
    Uncommitted changes
    , select the row of an uncommitted change to view the last committed version and the code of the uncommitted change.
  3. Select either:
    • Close
      . Retain all of the uncommitted changes in
      Uncommitted changes
      .
    • Discard uncommitted changes
      . Discard all of the uncommitted changes in
      Uncommitted changes
      . You cannot undo the discard of uncommitted changes. The changes saved to the local project are removed.
  4. (optional) If you discard uncommitted changes, the message
    The uncommitted changes will be removed from the project
    appears. Select
    Discard
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal