Edit an I/O mapping definition
Edit an I/O mapping definition to modify the name or device status when the device is
on or off.
IMPORTANT:
I/O mapping definitions apply to all lineups in a
project. Any changes to existing I/O mapping definitions impact all lineups that use the
definition.
- InI/O Mappingview, selectEdit I/O Mapping Definitions.
- InI/O Mapping Definitions, select the row of the definition and then selectEdit.
- InEdit I/O Mapping Definition, edit:
- Name. Type a new name for the definition.TIP: The definition name must be unique for I/O Type.
- Device Status when On. Select the desired status.
- Device Status when Off. Select the desired status.TIP: You can double-click a column entry to edit the name or device status for a definition.TIP: You cannot change the the I/O Type for an existing I/O mapping definition.
- SelectOKto apply the changes orCancelto not save the changes.
Changes to the I/O mapping definition are applied to all
lineups that use the definition.
Provide Feedback