View I/O mapping information
Open
I/O Mapping
to view detailed input and output
information about the selected device. From I/O Mapping
view you
can:- View and assign I/O mapping definitions to inputs and outputs for supported devices.
- View I/O Mapping definitions forDevice Status when OffandDevice Status when On.
- OpenEdit I/O Mapping Definitionsview.
- View the input and output on/off states for each input or output when status monitoring is enabled.
- View which devices do not support I/O mappings.
To view I/O mapping information
- On the explorer bar, select
Devices. - SelectIntelliCENTER.
- In theIntelliCENTERexplorer, double-click a lineup and then inElevationview, right-click a unit and selectI/O Mapping.TIP: To view mapping information from IntelliCENTER explorer, right-click a unit within a lineup and then selectI/O Mapping.TIP: To view mapping information from the unit profile, double-click a lineup, right-click a unit and then selectUnit Profile. Then at the bottom of the unit profile, select the device, theI/O Mappingtab, andI/O Mapping.
I/O Mapping
view displays input and
output mapping information. Provide Feedback