Delete an I/O mapping definition
Delete an I/O mapping definition to remove it from the definition from all lineups
that use the definition.
- InI/O Mappingview, selectEdit I/O Mapping Definitions.
- InIn I/O Mapping Definitions, select the rows of the definitions to remove.
- SelectDelete.
The selected I/O mapping definitions are removed from
I/O Mapping
view and all definitions that used the
definition.Provide Feedback