IntelliCENTER explorer

The
IntelliCENTER
explorer is a tree that depicts the hierarchical structure of the Motor Control Center Structure. Each level of the tree represents an element of the Motor Control Center:
When status monitoring is enabled and a device is in either a Warning, Fault or Communication Loss state, a appears at the Lineup, Section and Unit level. A path appears for you to find the device that has the potential issue. At the Device level, a status indicator appears. See Unit and device status indicators to view a list of indicators.
TIP: Context menus with options are available at each level of the IntelliCENTER explorer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal