Counter – Input View

Use Counter – Input to configure the Off → On and On → Off filter times for the different inputs.
Counter – Input View Example
The Counter – Input view includes these parameters:
Parameter
Description
Input A
Off → On Filter Time
Defines how long an Off to On input transition must remain in the On state before the device considers the transition valid.
Input A
On → Off Filter Time
Defines how long an On to Off input transition must remain in the Off state before the device considers the transition valid.
Input B
Off → On Filter Time
Defines how long an Off to On input transition must remain in the On state before the device considers the transition valid.
Input B
On → Off Filter Time
Defines how long an On to Off input transition must remain in the Off state before the device considers the transition valid.
Input A, B
Off → On Filter Time
Defines how long an Off to On input transition must remain in the On state before the device considers the transition valid.
Input A, B
On → Off Filter Time
Defines how long an On to Off input transition must remain in the Off state before the device considers the transition valid.
Input Z
Off → On Filter Time
Defines how long an Off to On input transition must remain in the On state before the device considers the transition valid.
Input Z
On → Off Filter Time
Defines how long an On to Off input transition must remain in the Off state before the device considers the transition valid.
Input00
Off → On Filter Time
Defines how long an Off to On input transition must remain in the On state before the device considers the transition valid.
This parameter is not visible if Input00 Function is set to Not Used in the Device Definition dialog.
Input00
On → Off Filter Time
Defines how long an On to Off input transition must remain in the Off state before the device considers the transition valid.
This parameter is not visible if Input00 Function is set to Not Used in the Device Definition dialog.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal