How is the maximum size of a data log configuration calculated?

Data cannot log if the resulting data log configuration exceeds the maximum size. Sample rate, number of tags, and log duration determine the size of a data log.
Each project contains up to three data logs.
View Designer
calculates the total size of all data logs in a project and compares the size against the maximum supported. The data logs in a project can have a combined maximum of 250 tags. Each data log can have up to a 500 millisecond sample rate and a 365 day duration.
If the data log fails project verification, reduce the size of one or more of the data logs by:
  • Reducing the log duration
  • Increasing the sample rate
  • Reducing the number of tags
The data log capacity used appears as a percentage in the bottom right corner of the data log .csv file.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal