Delete a data log from a project

Delete a data log from a
View Designer
project to stop the data log from collecting data on the HMI device. After deleting a data log, download the project to the HMI device. Deleted data logs cannot be undeleted. A
View Designer
project can contain up to three data logs.
To delete a data log from a project
  1. In the
    Project Explore
    r, expand the
    Data Logs
    folder.
  2. Right-click the data log and select
    Delete
    . The
    Project Explorer
    no longer contains the data log.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal