User-defined function blocks
Use the
User-Defined Function Blocks
node in Project Organizer to create logic programs for the Micro800
controller in the following languages:- Function block diagram (FBD)
- Ladder diagram (LD)
- Structured text (ST)
User-defined function blocks (UDFBs) define business logic for complex mathematical computations. Once created, it can be reused like other function blocks in
FactoryTalk Design Workbench
.Use the
User-Defined Function Blocks
node to:Use the
<UDFB-name>
node under User-Defined Function Blocks
to:- Open the UDFB Parameters window to:
- Create input or output parameters.
- Delete parameters.
- Move a parameter up or down in the UDFB.
- Edit the variable properties.
Provide Feedback