Import controllers, programs, function blocks, variables, or user-defined data types
Depending on the element type, the file formats for importing and exporting are different.
- The following elements are imported from an M8A file:
- Programs, including local variables and interrupts
- Function blocks, including local variables
- Functions, including local variables
- User-defined data types, including array data types, structure data types, and defined words
- Data logs
- Recipes
- The following elements are imported from a CSV or XLSX file:
- Modbus mappings
- MicroLogix mappings
- DNP3 mapping
- Global and local variables
Via CSV or XLSX files, you can manipulate the data and edit a large variable data set.
Provide Feedback