Rename an FBAxis
After adding a 2080-MOT-HSC plug-in module and activating it with
Feedback Axis
:- On the2080-MOT-HSCconfiguration page, aFeedback Axisnode is created. Select the node to view and configure the settings on the following pages:
- On the PTO Motion configuration page, aFBAxis<x>checkbox is added. The checkbox is selected and read-only by default.
Prerequisites
To rename an FBAxis
- InProject Organizer, go to , and then double-click2080-MOT-HSC.
- On the2080-MOT-HSCpage, selectFeedback Axis.
- On theFBAxis<x> - Generalconfiguration page, in theAxis namebox, enter the new name.
Provide Feedback