Hardware and software requirements

In the example project, an L70E controller is used. You can use an L20E or L50E controller instead.
The example project requires the following hardware and software components:
  • FactoryTalk Design Workbench
  • Ethernet driver, which is optional
  • L70E controller (2080-L70E-24QBB)
  • 24-volt DC power supply (2080-PS120-240VAC or equivalent)
  • 2080-MEMBAK-RTC2 plug-in module
  • 2080-IF4 plug-in module
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal