Configure Asset Training
- Output Frequency Min (Hz): Minimum VFD command frequency of the application
- Output Frequency Max (Hz): Maximum VFD command frequency of the application
- Advanced Settings
- Training Iterations (Default 100): The number of data trends received from the variable frequency drives from FactoryTalk Analytics GuardianAI. A lower value trains faster but generally results in a lower quality baseline. The recommended value to use is 100 iterations. The expected time taken to train the baseline will be between 11-18 minutes for each half hertz increment of the operation frequency.
- Trigger Value Hz (Default Empty): Advanced trigger configured for the drive high speed trend object. The value set will configure the drive to only send data to FactoryTalk Analytics GuardianAI for training/monitoring when the drive is operating at or above the frequency value set for the trigger. This parameter is used for advanced motion-based applications with the variable frequency drive. It will typically not be required when operating FactoryTalk Analytics GuardianAI on pumps, fans, and blowers.
NOTE:
The training performance may be impacted when running FactoryTalk Analytics GuardianAI on Windows via a Linux virtual machine. It is also recommended to place FactoryTalk Analytics GuardianAI as close as possible to the drive application to minimize the number of network hops.
Configure Training Parameters

Provide Feedback