Reset Ownership dialog box parameters

The
Reset Ownership
dialog box includes these parameters:
Parameter
Description
Password
The password field has these characteristics:
  • No minimum password length
  • 40 characters maximum password length
  • Is not case sensitive
Valid characters include:
  • Upper case A...Z
  • Lower case a...z
  • Numerals 0...9
  • Symbols ` ~ ! @ # $ % ^ & * ( ) _ + - = { } | [ ] \ : ; ? , . /
Reset Ownership
Resets the device to its factory defaults. The device is then owned by the user who successfully configures it next.
Resetting ownership causes all connections to or through the device to close, which might result in loss of control.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal