Configure Redundancy Module Options

On the Configuration tab of the
FactoryTalk® Linx
Redundancy Module Configuration Tool (RMCT), you can configure the following options for a redundancy module:
  • Auto-synchronization
  • Chassis ID
  • User program control
  • Fiber security
Redundancy Module Options
Redundancy Module Options
To configure redundancy module options, follow these steps.
  1. Access the RMCT.
  2. Select the Configuration tab.
  3. Select the configuration options for your redundancy application as described in the following sections.
  4. Select Apply.
  5. When the following message appears, select Yes to confirm the change.
    Confirmation message for configuration changes
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal