Configure Redundancy Modules
The default configuration of the redundancy modules enables you to synchronize the redundant chassis pair without additional configuration. If needed, you can configure the following:
- User-defined identification of the redundancy module
- Redundancy module options in theFactoryTalk® LinxRedundancy Module Configuration Tool (RMCT):
- Change the Auto-synchronization setting
- Assign a chassis ID
- Configure user program control
- Disable or re-enable fiber security
- Date and time settings
- Disable or re-enable SFP fiber ports
Provide Feedback