Port properties
Devices have logical ports that are associated with IP addresses, ports, and protocols.
Some of the following properties may be read-only for:
- The devices added to the Onboarding Area by Automatic Policy Deployment.
- The devices that are not added to a secure zone.
Device
This area displays information about the device on which the port is present.
Property | Description |
|---|---|
Device name | The name of the device. Select next to the device name to open the device properties. |
Device description | Read-only information that describes the device function. |
Device catalog number | Read-only information that provides the catalog number of the device. |
For more information, see Device properties.
General
Use this area to configure the port on the device.
Property | Description |
|---|---|
Port Name | The name of the port. |
Description | The optional description for the port. |
EtherNet Driver name | A dropdown list of the available EtherNet drivers used for communication. This property is only available for the devices that support CIP Security . The default name is Ethernet .If the list does not contain a driver, add the driver with FactoryTalk® Linx . |
Redundancy Status | Shows the redundancy status. If available, select Validate redundancy to validate the
redundancy status for the device. |
IP Address | The IP address of the Ethernet port, for example: 10.88.11.11 You cannot edit the IP address if you:
If the Clear configuration for previous IP Address dialog appears, either:
|
Port Proxied | Appears only for proxy devices. Shows the name and the IP address of the device secured by this proxy device. Select the pencil icon next to the device name to open the port properties. |
Proxy Device | Appears only for proxied devices. Shows the name and the IP address of the device securing this proxy device. Select the pencil icon next to the device name to open the device properties. |
Policies
Use this area to select the security zone and communication settings for the port.
Property | Description |
|---|---|
Zone | The name of the zone to which the port is assigned. If Automatic Policy Deployment is enabled, the Onboarding Area displays in the list of zones. |
Disable port HTTP (80) | For CIP Security capable devices only.When a device is CIP Security capable and placed in a zone using the certificate authentication method, the HTTP Port usage can be disabled.When viewing the device list, the Disabled TCP Port column reflects whether HTTP port 80 has been disabled. |
Property | Description |
|---|---|
Model Name | The name of the policy model managed by this instance of FactoryTalk Policy Manager . |
Inbound CIP Bridging |
|
Outbound CIP Bridging |
|
Provide Feedback