Device properties
Use device properties to define the device information, security, and network settings for a device.
Device properties defined using the electronic data sheet (EDS) for the device cannot be modified. A device can have one or more ports that are added to the policy model.
Some of the following properties may be read-only for:
- The devices added to the Onboarding Area by Automatic Policy Deployment.
- The devices that are not added to a secure zone.
Device
Property | Description |
|---|---|
Device Name | The name of the device. The name is required and must be unique. Generic devices are automatically named Device . Devices selected by catalog number or discovered are already named.<number> |
Description | An optional description for the device. The description of generic devices is empty by default. Devices selected by catalog number or discovered may have an existing description. |
Catalog number | If defined using device discovery, the catalog number cannot be changed.
Otherwise, choose a catalog number from the list. Choosing a Rockwell Automation catalog number automatically completes the Vendor
information.A device without a catalog number is listed as a Generic Device . |
Vendor | The name of the device's vendor. If a Rockwell Automation /Allen-Bradley catalog number was
provided, this setting is completed by default and cannot be modified. |
Firmware Revision | The firmware revision number of a device. Required to enable CIP Security for a device.This setting is required to apply CIP Security settings to the
device ports. FactoryTalk Policy Manager automatically assigns the latest
firmware revision to devices added using a catalog number or using
Discovery . |
CIP Security capable | Identifies whether a device can use the security settings of the zone. Select to configure additional CIP Security settings for a
generic device.The Catalog Number and firmware revision determine the CIP Security capability of a device automatically. |
Property | Description |
|---|---|
Disable CIP Bridging through USB | When selected, it disables inbound and outbound CIP Bridging through the USB port. When cleared, it enables inbound traffic through the USB port. Outbound traffic is enabled if the device supports it. This setting is only
available for the devices with the Capable property
enabled. The available options may be restricted by FactoryTalk Policy Manager
Settings.
TIP:
This property is read-only for redundant
pairs. See Redundancy system.
|
Property | Description |
|---|---|
Port name and number | The name and number of ports available on the device. Select next to the port number to configure
port properties, such as the port name, description, EtherNet driver, IP address,
and protocols used by the device. For more information, see Port properties. |
TIP:
For generic devices, you can manually add ports as needed by selecting
+
next to Ports
.For
CompactLogix
5380 Controllers and Compact GuardLogix
5380
Controllers that operate in dual mode, you cannot add Port 2
.Mobile connectivity
Item | Description |
|---|---|
Set PSK | Set a Pre-Shared Key (PSK) and PSK ID for mobile connectivity to manage
supported devices through the . See Set PSK for mobile connectivity. |
Reset PSK | Reset PSK and PSK ID for supported devices configured for mobile connectivity.
See Reset PSK for mobile connectivity. |
Rename PSK ID for supported devices configured for mobile connectivity. See Rename PSK ID for mobile connectivity. | |
Delete PSK and PSK ID from supported devices configured for mobile connectivity.
See Delete PSK and PSK ID from a device. |
UA Client
Item | Description |
|---|---|
Name | client name.
TIP:
The default
UA Client tab title changes if
you change the client name. |
IP Address | IP address of the client. |
Item | Description |
|---|---|
Zone | The zone that the client is assigned to. |
Item | Description |
|---|---|
Export | Exports the client certificate. |
Import | Imports the client certificate. |
Item | Description |
|---|---|
Sharing identity with the server | client shares its identity with the server identity. The identity includes the PKI
certificate, username, and password. |
UA Server
Item | Description |
|---|---|
Name | server name.
TIP:
The default
UA Server tab title changes if
you change the server name. |
Server URI | Non-editable server URI based on the server certificate. |
Server URL | The URL of the server endpoint. |
Endpoint | List of endpoints with the Sign & Encrypt security policy mode or stricter. For more information, see OPC UA security policy. Select Refresh to refresh the list. |
Endpoint Encryption to use for Deployment | Encryption algorithm for the server endpoint
to use for deployment.
TIP:
The encryption algorithm may change if you specify a different endpoint in
Server URL . |
Item | Description |
|---|---|
Zone | The zone that the server is assigned to. |
Item | Description |
|---|---|
Anonymous | Log on as an anonymous user to the server. |
Username | The user name to log on to the server. |
Password | The password to log on to the server. |
Show Password | Shows the password. |
Item | Description |
|---|---|
Import | Imports the server certificate. |
Item | Description |
|---|---|
Verify | Verifies connection to the server. |
Sharing identity with the client | server shares its identity with the client identity. The identity includes the PKI
certificate, username, and password. |
Gateway
Item | Description |
|---|---|
Refresh List | Refreshes the list of nodes associated with the gateway. |
Properties | Opens node properties. See Node. |
Replace device | Replaces the node device. See Replace a device. |
Resets node device configuration to factory defaults. See Reset a node. |
Node
Item | Description |
|---|---|
Back to Policy Gateway | Opens properties of the associated gateway. See Gateway. |
Item | Description |
|---|---|
Device Name | Device name of the gateway that the node is connected to. Select
Properties to edit gateway properties. See Gateway. |
Product Name | Product name of the gateway that the node is connected to. |
Product code | Product code of the gateway that the node is connected to. |
Item | Description |
|---|---|
Port Name | Node port name. |
Description | Node description. |
IP Address | Node IP address. |
Item | Description |
|---|---|
Zone | The zone of the associated gateway. |
Provide Feedback