Add discovered devices

Add the discovered devices the device list and assign them to zones.
TIP:
Discovery
can show multiple child devices under one CIP Proxy device when a security policy is not yet deployed to the CIP Proxy device. After security policy deployment,
Discovery
shows only the proxied device as a child.
To add a device manually, see Add a device.
Prerequisites
Enable automatic device discovery. See Configure automatic device discovery.
  1. To add discovered devices
  2. From the navigation bar, either:
    • Select
      Canvas
      and then select a zone or
      Unassigned
      to contain the device.
    • Select
      Zones
      and then select a zone to contain the device.
    • Select
      Devices
      to contain the device in the devices list not assigned to any zones.
  3. In
    Discovery
    , select either
    CIP
    or
    OPC UA
    .
  4. (optional, CIP only) Enable or disable
    CIP Security
    indicators by selecting shield
    Show CIP Security Indicators
    from the toolbar.
    For more information, see Discovery pane.
  5. (optional) Filter the list of discovered devices.
    For more information, see Search discovered devices.
  6. Either:
    • In
      Discovery
      , select a device or multiple devices and then select .
    • In
      Discovery
      , right-click a device and select
      + Add
      .
    • Drag a device from
      Discovery
      to the table in
      Zones
      or
      Devices
      .
    • Drag a device from
      Discovery
      to a zone or
      Unassigned
      in
      Canvas
      .
The selected discovered devices are added to the zone or unassigned devices list.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal