Configure automatic device discovery
Enable or disable the automatic discovery of CIP or OPC UA devices in the
Discovery
pane.- To enable the automatic discovery of CIP devices:
- InDiscovery, selectCIP.
- Select to enable or disable the automatic discovery of CIP devices.
- To enable the automatic discovery of OPC UA devices:
- InDiscovery, selectOPC UA.
- Select to enable or disable the automatic discovery of OPC UA devices.
Provide Feedback