Verify time synchronization

To verify time synchronization
  1. Open the web browser and type
    https://<Module IP_address>:8443
    .
    The FactoryTalk Historian ME Web Diagnostics client appears.
  2. Click the
    Hardware
    tab, and then click
    Time Management
    .
    The
    Time Management
    page appears.
  3. Under
    Time Management
    , verify the settings for the NTP server computer.
If there are any problems with the synchronization, an error message appears next to the
Time Source
box.
Verify time synchronization 1
The time synchronization status is additionally indicated by:
You can find additional details about the synchronization under
NTP Logs
.
Verify time synchronization
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal