Home

The
Home
tab displays the following information:Item | Description |
|---|---|
Device Name | The name of FactoryTalk Historian ME . |
Device Description | The version number of FactoryTalk Historian ME . |
Device Location | The physical slot location of the FactoryTalk Historian ME module in the chassis. |
Ethernet Address (MAC) | The MAC address of the Ethernet port. |
IP Address | The IP address of FactoryTalk Historian ME . |
Production Revision | The revision number of FactoryTalk Historian ME . |
Firmware Version | The version number of the firmware. |
Serial Number | The serial number of FactoryTalk Historian ME . |
Up Time | The amount of CPU time used. |
Provide Feedback