Use Web Diagnostics

In this chapter, you will learn how to troubleshoot and tune your Historian ME module using the FactoryTalk Historian ME Web Diagnostics page.
FactoryTalk Historian ME is an embedded system with multiple layers of firmware applications. Firmware applications and hardware components are available via the FactoryTalk Historian ME Web Diagnostics page.
To access the Web Diagnostics page
  1. Open the web browser and type
    https://<Module IP_address>:8443
    .
    TIP:
    You can also use the Fully Qualified Domain Name instead of the IP address of the module. Type the domain name in the following format:
    <modulename>.<domainname>.<top-level domain>
    For example,
    module1.mycompany.com
  2. In
    Windows Security
    , type the user name
    admin
    and the password
    admin
    .
    TIP:
    This is an optional step if the module is in safe mode. You can repair archives without login. For more details, see Repair archives using safe mode.
  3. Change the password for the default
    admin
    user.
    For more details, see Change password.
The page contains the following tabs:
  • TIP:
    • To open the web diagnostics online help, click
      Help
      .
    • To check the firmware version and product ID, click
      About
      .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal