Startup log

The
Startup Log
page lists logs recorded each time the module is rebooted.
To search the startup log
  1. In the
    Time
    text box, type the time parameters.
  2. In the
    Source
    text box, type the source you want to search for.
  3. In the
    Message
    text box, type the type of message you want to search for.
  4. In the
    Count
    text box, type the maximum number of records you want the search to return.
  5. Click
    Search
    . The selected records appear in the list on the Startup Log page.
    TIP:
    For details on time options, see Set start and end times.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal