Set start and end times

The start and end times are set in relation to the time on the client computer.
The default start time is two minutes before the current time on the client computer. The default end time is the current time on the client computer.
You can use the following expressions to set time:
This expression
Means
*
The current time.
t
Today at midnight (00:00:00).
y
Yesterday at midnight (00:00:00).
t 15:00:00
Today at 3:00:00 pm.
y 15:00:00
Yesterday at 3:00:00 pm.
-60s
The past 60 seconds.
+45m
The future 45 minutes.
-5h
The past 5 hours.
-3d
The past 3 days.
sun
The most recent Sunday at midnight (00:00:00).
25 8
08:00 on the 25th of the current month.
25 8:10
08:10 on the 25th of the current month.
06-dec-08 15:00:00
3:00:00 p.m. on December 6, 2008.
mon+14.5h
2:30:00 p.m. last Monday.
sat-1m
11:59:00 p.m. last Friday.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal