Restore the module's defaults
TIP:
You must have administrator privileges to restore the module.
When you restore the module, all data stored on FactoryTalk Historian ME is deleted, including any backed up configuration file. Make sure that you download the backup configuration file(s) before restoring FactoryTalk Historian ME. For details, see Restore the module from the backup file.
To restore FactoryTalk Historian ME to its original configuration
- Click theAdvancedtab, and then clickRestore Defaults.TheRestore Defaultspage appears.
- ClickRestore Defaults.FactoryTalk Historian ME is restored to its default settings.
When you restore the module to the default configuration, you must also restart all module clients (for example, FactoryTalk Historian DataLink, FactoryTalk Historian ProcessBook, FactoryTalk View SE Trending, PI System Management Tools (SMT), or PI SMT Tag Configurator).
TIP:
- Alternatively, you can perform the Restore Defaults and Reset Security actions on your Historian module in the Logix Designer Module Profile.If the Restore Defaults or Reset Security actions are being executed in the Module Profile, you will not be able to restore the default settings, reset the security configuration, or reboot the module from the web client.For details, see Configure the module properties.
- After restoring the module to the default configuration, change the password for the defaultpiadminuser.For more details, see Change user passwords.
Provide Feedback