Change user passwords
Any user can change their own password, but only members of the
piadmin
group can reset passwords for other users.To change the user password
- On theUser Managementpage, highlight the user whose password you want to change.
- ClickChange Password.
- Do one of the following:
- If you are changing your own password, type the old password in theOld Passwordtext box.
- If you are changing another user's password, type "!" in theOld Passwordtext box.
- Type a new password or leave the text box blank.The password must be any combination of lowercase and uppercase characters (a-z, A-Z) and digits (0-9).
- Confirm the new password.
- ClickSave.
Provide Feedback