Reset the default admin password

If the default administrator (
piadmin
) password is lost or forgotten and you cannot make administrator-level changes to FactoryTalk Historian ME, you must reset the
piadmin
user password and security settings.
To reset the default admin password
  1. Click the
    Advanced
    tab, and then click
    Restore Defaults
    .
    The
    Restore Defaults
    page appears.
  2. Click
    Reset Security
    .
    A message appears asking you to confirm the action.
  3. Click
    OK
    .
You can now access default administrator functions. The default password for the
piadmin
user is empty. It is important to change the default
piadmin
password after you log on.
TIP:
You can also reset the password from the Logix Designer interface. For details, see Configure the module properties.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal