Upload the backup file to the module
To upload the backup file from the client computer to the module
- Click theConfigure Historiantab, and then clickBackup And Restore.TheBackup and Restorepage appears.UnderUpload to Module, the details of the last upload are displayed:
- The time the backup file was last uploaded to the module.
- The name of the last uploaded backup file.
- ClickBrowse.
- Locate the file you want to upload, and then clickOpen.
- ClickUpload.TIP:
- You can also upload the backup file downloaded from one FactoryTalk Historian ME Module to quickly configure another FactoryTalk Historian ME Module.
- Please take the following into consideration:
- You can only have one backup configuration file at a time on the FactoryTalk Historian ME Module.Only the last version of the backup configuration is stored.
- The name of the backup file may not exceed 80 characters.
- The backup file must contain the.tar.gzextension in its file name.
- If you upload an older backup file, it will overwrite any newer backup file.
- The backup file cannot contain a space in its name.
Provide Feedback