Back up and restore configuration files
We recommend that you periodically back up the module configuration. You should also back
up the configuration whenever changes are made to it. In case you need to reset the module,
you will be able to restore the configuration after the module resets.
This table describes the backup configuration that can be restored on which Historian module series.
Backup configuration | Can be restored on |
|---|---|
Series A | Series A, B, or C |
Series B | Series B or C |
Series C | Series C |
TIP:
You must have administrator privileges to back up or restore the module's configuration
files.
Provide Feedback