Export data

You can export all points that are listed in your search results. The data is exported to a CSV (comma-separated values) document that you can open in Microsoft Excel.
To export data
  1. Find the data that you want to export by defining your search criteria.
    For details, see Define search criteria.
  2. Export data.
    To export all the data displayed in the search results
    • Click
      Export
      .
      To export specific data
    • Select a checkbox in the
      Select
      column next to the data row that you want to export.
    • Click
      Export
      .
      The
      Save HTML Document
      dialog box appears.
  3. Navigate to the place in which you want to save the file.
    If you change the name of the file, make sure to leave the
    .csv
    file extension in the
    File name
    box.
    Leave the default settings in the
    Save as type
    and
    Language
    boxes.
  4. Click
    Save
    .
    TIP:
    The FactoryTalk Historian DataLink Excel Reporting Tool provides a Historian Add-In for Microsoft Excel. If you export more than 65,535 rows of FactoryTalk Historian ME events to FactoryTalk Historian DataLink using the Compressed Data (Start Time/End Time) configuration page, Excel generates an "r;Output exceeds dimension" message.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal