Create point discovery rule files
Instead of using the default point discovery rule file, you can create your own.
To create a point discovery rule file
- Go toStart > All Programs > Rockwell Software > FactoryTalk Historian ME Rule Editor > Launch Rule Editor.The FactoryTalk Historian ME Rule Editor window appears.
- UnderFile Management, clickRule File Management.TheFactoryTalk Historian ME User Defined Rule File Listdialog box appears.
- ClickNew.TheFactoryTalk Historian ME User Defined Rule Filedialog box appears.
- UnderRule File Name, type a name for the rule.When typing the name, keep in mind the following points:
- The file name may only contain the following characters: @, ., -, _, a-z, A-Z, 0-9, and must not contain any spaces.
- You may include the "Rule_" phrase at the beginning of the name, however, only once.
- You cannot include the "Rule_" phrase inside the rule name.Adding it will cause problems with creating and viewing the rule file.
- (optional) UnderDescription, type a description for the rule.
- ClickOK.The rule appears in theFactoryTalk Historian ME User Defined Rule File Listdialog box.
- Select the rule, and then clickOpen.The rule file is listed underCurrent Rule Filein theFactoryTalk Historian ME Rule Editorwindow.The following information is provided in the current rule file:
- The file name.The name of the rule file that you have typed when creating the file is prepended with theRule_prefix, unless you have already included it while naming the rule.
- The description.The point discovery rule files are stored in the following location:C:\Users\<User Name>\Documents\Rockwell Automation\RuleEditor\The names of the custom point discovery rule files are preceded with aRule_ prefix.
Now you can add components to your rule file. For details, see:
Provide Feedback