Add an Ethernet driver
After installing the Module Profile, make sure that you install and configure an Ethernet driver using RSLinx Classic. You will use the driver to connect to your processor and download the Ladder logic to the controller.
For details, see the RSLinx Classic user documentation.
To add the Ethernet driver
- Go toStart > All Programs > Rockwell Software > RSLinx > RSLinx Classic.RSLinx Classic appears.
- On theCommunicationsmenu, clickConfigure Drivers.TheConfigure Driversdialog box appears.
- In theAvailable Driver Typeslist, clickEthernet devices.
- ClickAdd New.TheAdd New RSLinx Classic Driverdialog box appears.
- In the text box, type the name of the Ethernet module (ENBTorEN2T) from your chassis.
- ClickOK.TheConfigure driverdialog box appears.
- Next to the 0 station, type the IP address of the Ethernet module (the leftmost module).
- ClickOK.The new driver appears underConfigured Drivers.
Provide Feedback