Example: Use the Module Profile

In this example, you will learn about the following:
  • Setting up a controller in the local chassis to monitor key FactoryTalk Historian ME statistics, and control the data collection service using the Module Profile.
  • Writing the controller logic for:
    • Monitoring key statistics of the Historian module with input tags.
    • Making control decisions using output tags.
      You can use the output tags to control the status of the data collection (running or stopped) and the status of the Historian module (running or shut down).
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal