Data collection issues
Symptom | Solution | |
|---|---|---|
The System Status section on the Home page shows that the data collection is in the "Stopped" mode. |
| |
|
| |
The System Status section on the Home page shows that the data collection is in the "Error" mode. |
| |
Tags are collecting bad-quality data. | If you change a tag's external access attribute to none , then the data
collected by that tag for FactoryTalk Historian ME will be bad quality. To fix
this issue, you must change the tag external access attribute to either
Read/Write or Read only . | |
Snapshot data points displayed on the Current Data page contain timestamps that are not being updated. | Check the status of the data collection on the Home page. | |
Go to Time Source > Controller in the web interface. Check for a message that indicates that data collection has discarded data. | ||
If the data collection status is "Running", check the Collection Rate in the System Status section in the left navigation bar. | ||
|
| |
If the data collection status is "Stopped", go to the Data Collection page and restart the data collection. | ||
A single point has not collected data for a significant time period. |
| |
The module receives a high-speed event with a timestamp 10 minutes into the future, discards that event, and logs the following error message into the system log: [ERROR] TagProcessingForPolledAndAdvised() dropped future event for point<ID> with <timestamp> with timeDelta=<number of seconds into future>. |
| |
The following message is logged on the System Log page:[ERROR] Unable to keep pace with High Speed Trend causing data loss. | Due to performance issues with the controller, the backplane, or the module, the module cannot receive new high-speed events from the controller. To mitigate the impact, stop and restart the data collection. | |
Provide Feedback