Reboot the module
FactoryTalk Historian ME can be rebooted in two ways:
- In the web interface, go toAdvancedin the top navigation bar, and then clickModule Shutdownin the left navigation bar. ClickModule Rebootto reboot the module.For details, see Reboot the module.
- In the Logix Designer Module Profile, clickReset Module.For details, see Use Studio 5000 Logix Designer Module Profile.
Provide Feedback