Auto recovery issues

Symptom
Solution
The time on the module has moved to a past time. This causes existing archives to have future timestamps or overlapping archives.
  • First, check the module's time source to ensure that it is correct. To resolve time source issues, see Time management issues.
  • If the issue is not a time source issue, restore the module to its proper state by rebooting it. The module will start in safe mode.
  • Click
    Safe Mode
    which initially appears when the module is rebooted. (Safe Mode indicates that your system is in safe mode.)
  • Download archives to retain the archive data for your records.
  • Next, delete the archives with future timestamps or overlapping archives. For details, see Repair archives using safe mode.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal