Integrate the module into a FactoryTalk environment with FactoryTalk Directory
In this section, you will learn how to integrate a standalone FactoryTalk Historian ME module into an existing FactoryTalk system using FactoryTalk Directory. Integrating a standalone module into an existing FactoryTalk system allows:
- Centralized administration of security credentials, performed in FactoryTalk Administration Console.
- FactoryTalk clients (for example, FactoryTalk View SE or FactoryTalk Batch) to connect to the FactoryTalk Historian ME module.
Provide Feedback