Review results
This is step 3 of adding points using the Add Points Wizard
The
Review Result
wizard page contains information on the points that have been processed.The page contains the following information on points:
- The number of points that were created is based on the tags that you have selected on theCreate pointswizard page (See Create points).
- The number of points that were not created because of either of the following reasons:
- A specific point already exists in the archive.
- An error occurred.For details, see System log related issues.
- The total number of points in the module, including the newly created ones.
The points that have not been created are listed in the
Points Not Created
table, along with an explanation for the point creation failure.Once you finalize the data point creation, restart the data collection by clicking
Restart Data Collection
. The process may take several minutes.
TIP:
If the FactoryTalk Historian ME Module receives an event with a timestamp 10 minutes or more into the future, it will discard that event and log an error message in the system log as follows:
[ERROR] TagProcessingForPolledAndAdvised() dropped future event for point<ID> with <timestamp> with timeDelta=<number of seconds into future>
For example:
6-Oct-09 15:54:29 Data Collection [ERROR] TagPr
ocessingForPolledAndAdvised() dropped future event for point 450 with timestamp 13-Oct-09 00:37:03.89001 with timeDelta=549754
Note that if the data transfer service is in the auto transfer mode, it may continue running. If the auto transfer mode is not enabled, you must manually select points to transfer, and then restart the data transfer service.
Provide Feedback