System log related issues

Keep in mind the following system log related issues:
  • If you are using IE 7.0 and want to export to Excel, you must install Windows hotfix 929863. This fix addresses an Excel file export issue on the
    System Log
    page. You need to add the
    [HKEY_CLASSES_ROOT\.csv] "PerceivedType"="document"
    registry value for the .csv document type.
  • If you use the
    Auto Refresh
    feature, new messages will appear in the
    System Log
    table each time data is refreshed. When multiple clients perform the refresh action, the
    System Log
    table will grow quickly.
  • When the FactoryTalk Historian ME systems are up and running, and the connection to the data source is lost, a message similar to the following will be logged:
    0 DataCollection 28-Dec-09 19:00:47 [ERROR] HandleNotification() detected erroneous return condition from notify_on_event API
    .
    This message is logged every 300 errors to help prevent the log disk space from being filled with too many error messages.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal