Use the system log

To search for messages reported to the system log, and export the search results
  1. Click the
    Advanced
    tab.
    The
    System Log
    page appears.
  2. Review the following for additional information.
    Item
    Description
    Time
    Use the
    Time
    box to specify time search criteria. The table uses
    m
    for minutes and
    d
    for days. The default value is
    *-5m
    .
    Source
    Use the
    Source
    box to filter by source.
    The default value is "*", which means that no filtering is used and messages from all sources are displayed.
    Message
    Use the
    Message
    box to filter by message text.
    The default value is "*", which means that no filtering is used and all messages are displayed.
    Count
    Use the
    Count
    box to limit the maximum number of log messages that will be searched out.
    The default value is 1000. The maximum value that you can enter is 5000.
  3. Specify the search criteria.
  4. Click
    Search
    to display the messages using the criteria specified.
    The messages are displayed in a table. By default, the messages are displayed sorted by time, from oldest to newest. You can sort the messages by heading. For example, click the
    Source
    heading to sort the messages by source alphabetically, in ascending order.
  5. Click
    Export
    to export all search results to a file.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal