Shut down the module

The module shutdown allows you to stop all FactoryTalk Historian ME-related services (including the point server, the data collection, the data transfer, and the web configuration server). It is recommended that you shut down the module if you plan to remove it from the chassis or if you are going to power down the chassis.
To shut down the module
  1. Click the
    Advanced
    tab, and then click
    Module Shutdown
    .
    A message appears asking you to confirm the action.
  2. Click
    OK
    .
    The module shutdown is complete when the scrolling message on the module displays the module's IP address followed by SHUTDOWN.
    TIP:
    Alternatively, you can shut down the module using the FactoryTalk Historian ME Logix Designer Module Profile.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal