Edit points

To edit points
  1. Click
    Manage Points
    , and then click
    Edit Points
    .
    The
    Edit Points
    page appears.
  2. Using the search boxes, set your point search criteria, and then click
    Search
    .
  3. In the search results table, click the point that you want to edit, and then click
    Edit
    .
    The
    Point Property
    page appears.
  4. Change the point attributes.
    For details, see Define point attributes.
    If you want to cancel your changes and bring back the original attributes of the point, click
    Reset
    .
    TIP:
    Resetting will not work after you save the changes using the
    Save
    button.
  5. Click
    Save
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal